Article Reprints
Have you ever wanted to easily track changes made to your Keysight Technologies, Inc. Medalist i3070 test program? Enhanced Log Records is a set of tools on the Medalist i3070 board test systems at software revision 7.10p that monitors and validates whether the board directory contents have been modified, including the testplan in memory. A report can be generated that includes the date and time that a file was changed. This can help to easily identify what changes have been made to your program.
Baselining
Baselining is part of a methodology that tracks when the programming changes occur and establishes markers when such changes have been approved. Baselining is especially important during board test production runs as it tracks and reports when and where files have been changed as boards are tested. Such tracking capabilities help assure test confidence and quality by validating that the tests released into production are continually monitored throughout the manufacturing life cycle.
All board test object files under a board test directory are baselined. Baselining records the filename, its CRC, and a timestamp in a custom database that resides in the board directory. As a function of board test runtime, object files are loaded as they are executed. At this time, the object files are cross-checked with their baselined CRCs in the database. If there is a mismatch, an alert record is generated. Also, the loaded testplan is cross-checked with its recorded CRC when the testplan is run. Furthermore, the loaded filename is checked with its recorded name and CRC when that program is run. This verifies that the loaded testplan was not edited in memory and then run.
The standard data log record format is used as the alert record that a change occurred. As part of the board start/board end log record, it reports general quality control health – good and bad state information. It provides a level of encryption within the data log content so that it is constantly changing and near impossible to compromise. This encrypted record describes the file indicted from the CRC mismatch.
By default, baselining is disabled on a board test directory. The article describes how to enable and use the baseline feature.
Procedure
Step by step procedures to enable the enhanced log records in a board directory
Conclusion:
Now, when a test program change is detected during production, a log record is generated detailing this change event so that the change can be properly reviewed. Using a change control process, such an event may either be accepted or corrective action may be taken
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.