Case Studies
Standalone Bypass Supports Fail-Safe Operation of Cisco Security Appliance
After a demonstration that showed information leaving the company and going to China in an unsecure fashion, this Global 500 manufacturer of HVAC equipment and automotive devices received CFO approval to purchase the appliances necessary for inline security monitoring.
They chose the Cisco ASA with FirePOWERTM for its advanced functionality, and the network team looked for a way to support real-time monitoring, while also protecting network availability. Ixia provided the solution they needed.
The Need for Failover
The company’s previous firewall solution failed closed – meaning that if it lost power or stopped functioning, traffic was not forwarded on.
However, Cisco’s ASA with FirePOWER needs to be able to fail open. It must be set up in a way that permits network traffic to continue flowing, even when the device goes down. This is because ASA FirePOWER is more than just a firewall.
It brings an Intrusion Prevention System (IPS) and a Next Generation Firewall (NGFW) together, in a single device. FirePOWER appliances must fail open and keep traffic flowing to allow:
• IPS policies to be reconfigured
• The appliance to be serviced or upgraded
• The appliance to be moved from one network segment to another
... all without impacting network traffic and causing costly network downtime.
Ixia’s external bypass switch is designed to do exactly that using the industry’s fastest heartbeat, to fail open as fast as possible in the event of a failure. Using a bypass switch in tap mode also allows the IPS to function as an Intrusion Detection System (IDS) – passively monitoring network traffic without affecting it, for even more flexibility.
Fastest Time to Value
The company did a head-to-head comparison of multiple bypass solutions and chose the Ixia iBypass VHD, the highest density bypass switch available. Fast, accurate deployment was essential, as the company wanted to implement security appliances in over 1000 locations across six continents. A slow complicated process would have cost the manufacturer too much time and disrupted business. Ixia’s solution helped them avoid this.
Ixia’s iBypass is preconfigured to automatically integrate with Cisco security appliances via a single click, to limit potential configuration errors and deploy tools in minutes, instead of hours.
Control and Configuration Made Easy
Ixia iBypass switches were deployed along with Ixia Indigo Pro: a centralized system for configuration and management of an organization’s taps, bypasses, monitoring switches, and network packet brokers. With dozens of bypasses installed in multiple locations across the globe, the company needed a streamlined and cost-effective way to manage them all remotely, from a single pane of glass.
Indigo Pro allows the company to push configurations and updates to every device – across the globe – at the touch of a button. According to the network team, Ixia’s competitors were unable to offer this level of functionality. Without Indigo Pro, they would have been forced to update, revise, patch, or push configurations to each device, one by one. Indigo Pro was a key component of the deployment process, saving the company hours of IT admin. Furthermore, the network team was particularly impressed with the highly-visual user interface that Ixia offered, in contrast to competitive solutions.
Können wir Ihnen behilflich sein?