WLAN - X-Series Signal Analyzers Python Instrument Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Plattform wählen :

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2024-04-04 1.0.1 Initial public release
Veröffentlichungsdatum Version
2024-04-04 1.0.1
Version Description
Initial public release

Driver type: Python (32-bit/64-bit)

Python Version Support: 3.6 - 3.10

Prerequisite: keysight_ktxsan Python Driver

 

Driver Download Options

  1. Binary Packages for supported Python versions
  2. Source Package

 

Wie geht das Herunterladen

  1. Click the Download button
  2. Download the package

 

How to Install

 

  • Binary Package
    1. Copy the downloaded package (archive file) to a temp folder
    2. Unzip the file
    3. Perform one of the following options:
      • If the prerequisite keysight_ktxsan Python Driver is not installed, run “install.bat” file either directly or via command prompt
      • If the prerequisite keysight_ktxsan Python Driver is installed, use the “pip install” command to install keysight_ktxsanwlan driver only. For example, >> pip install keysight_ktxsanwlan-1.0.1-cp38-cp38-win32.whl
 
  • Source Package
    1. Distributed source package means when the user runs pip install <package_name>, the binary package is built and installed from the source package, compatible with the user’s environment. Important to note users cannot modify python driver APIs. 
    2. Prerequisites 
      • Python 3.6 to 3.10
      • C++ Compiler: MSVC compiler. Install Visual Studio (any edition) with "Desktop development with C++" workload selected  OR  if full VS ADE not needed, Build Tools for Visual Studio (command line interface) with "C++ build tools" workload selected. 
      • CMake 3.16 or newer: CMake tools are used to build and install the driver Python module. If needed, install the latest stable binary distribution for Windows or Linux from CMake.org.  
      • VISA: The driver module uses VISA to communicate with the instrument. Any compliant implementation is acceptable. The latest version of Keysight IO Libraries Suite is recommended, includes VISA. 
    3. Copy the downloaded package to a temp folder 
    4. Unzip the file
    5. Perform one of the following options:
      • If the prerequisite keysight_ktxsan Python Driver is not installed, run “install.bat” file either directly or via command prompt
      • If the prerequisite keysight_ktxsan Python Driver is installed, use the “pip install” command to install keysight_ktxsanwlan driver only. For example, >> “pip install keysight_ktxsanwlan-1.0.1.tar.gz”.

 

Lizenzierung

  • Does Not Require a License

Installs on: PC

Betriebssystem

  • Windows 11
  • Windows 10
  • Windows 8.1/8
  • Windows 7 SP1

Note: Python 3.9 is NOT supported on Windows 7.

 

Supported Instruments

  • N9000A, N9010A, N9020A, N9030A, M9420A, N9020B, N9010B, N9000B, N9030B, N9040B, N9041B, SPN9003A, SPN9026A, M9421A, M8920A, M90XA, M9410A
Keine Softwareversion verfügbar
SHOW MORE