The KS83MX0A Soft Front Panel enables remote control of the V3060A E-Band 60-90 GHz transceiver, used in automotive radar testing.

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Kostenlos Trial
Veröffentlichungsdatum Version Versionsbeschreibung
2026-06-09 1.3.1 New features - Custom cable length support in RTS mode
Veröffentlichungsdatum Version
2026-06-09 1.3.1
Version Description
New features - Custom cable length support in RTS mode

Highlights of V3060A Soft Front Panel 1.3.1

New Features
  • Custom cable length support in RTS mode.

Wie geht das Herunterladen

  1. Click the Download button.
  2. Save the file to a folder on C drive of your PC.

How to Install

  1. Install Keysight IO Libraries Suite.
  2. Install Keysight License Manager.
  3. Install V3060A Soft Front Panel: Double-click the V3060A_SoftFrontPanel.exe file and follow the instructions that appear in the installation window wizard until the installation is completed.

Lizenzierung

  • Requires a license.

Installs on: PC

Betriebssystem

  • Windows 10 and above

Highlights of V3060A Soft Front Panel 1.3.0

New Features
  • Added Best simulated RCS flatness VS frequency capability.
  • Added Estimated RF Power at Tx/Up port.
  • Added LED indicators to show signal presence on the V3060A module.

Enhancements

  • Enhanced the RF Center Frequency field to support a more flexible input.
  • Enhanced the Doppler Frequency input to 1 Hz resolution.

Wie geht das Herunterladen

  1. Click the Download button.
  2. Save the file to a folder on C drive of your PC.

How to Install

  1. Install Keysight IO Libraries Suite.
  2. Install Keysight License Manager.
  3. Install V3060A Soft Front Panel: Double-click the V3060A_SoftFrontPanel.exe file and follow the instructions that appear in the installation window wizard until the installation is completed.

Lizenzierung

  • Requires a license.

Installs on: PC

Betriebssystem

  • Windows 10 and above

Wie geht das Herunterladen

  1. Click the Download button.
  2. Save the file to a folder on C drive of your PC.

How to Install

  1. Install Keysight IO Libraries Suite.
  2. Install Keysight License Manager.
  3. Install V3060A Soft Front Panel: Double-click the V3060A_SoftFrontPanel.exe file and follow the instructions that appear in the installation window wizard until the installation is completed.

Lizenzierung

  • Requires a license.

Installs on: PC

Betriebssystem

  • Windows 10 and above
SHOW MORE