Solution Briefs
Avionics electronics form the backbone of modern aircraft operations, supporting mission-critical systems such as radar, communications, flight control, navigation, fire control, and sensor modules. These devices must perform reliably through rapid power changes, engine start conditions, electrical disturbances, and dynamic load transitions. Ensuring their operational integrity requires a test environment that accurately replicates real aircraft power behavior while safeguarding expensive, highly sensitive DUTs. This solution brief presents how Keysight ATE system power supplies provide an integrated approach to avionics power testing—combining precision power sourcing, advanced DUT protection, programmable transient simulation, automated sequencing, and synchronized high-speed measurement.
Avionics power validation is uniquely challenging due to the extreme variability and sensitivity of aircraft electrical systems. During ground-to-engine power transfer, engine start-up, or power-bus switching events, transient disturbances can be sharp and unpredictable. Avionics modules are exceptionally vulnerable to overstress during turn-on, especially if sequencing, slew rate, or timing is uncontrolled. Engineers also require the ability to capture fast inrush currents, voltage dips, surges, and transient anomalies—events that often occur within microseconds and cannot be analyzed without synchronized digitizers and pre/post-trigger capture. The absence of continuous data logging makes root-cause analysis even more difficult, particularly when faults or unexpected shutdowns occur during long-duration test cycles.
Keysight’s solution addresses these challenges using a unified platform that merges sourcing, measurement, protection, and transient generation into a single ATE-ready system. Engineers can apply arbitrary waveforms that replicate real aircraft disturbances such as dropouts, surges, voltage interrupts, engine-start transients, switching noise, or power-bus instability. This allows for realistic and highly repeatable qualification testing without external switching racks or standalone transient generators. Controlled slew rate and coordinated multi-channel sequencing ensure safe, consistent turn-on behavior for avionics modules, reducing the risk of overstress during startup procedures.
The platform also integrates fast, high-resolution voltage and current digitizers that enable deep insight into system behavior. Engineers can capture inrush current, transient load dynamics, voltage recovery characteristics, and pulse-to-pulse variation with microsecond-level detail. Background data logging functions as a built-in “power test flight recorder,” storing historical measurements and events so that investigations into anomalies can proceed quickly and accurately. These capabilities are essential for understanding how avionics subsystems respond to real-world electrical stresses and for ensuring that mission-critical behavior remains stable under all conditions.
The example use case presented in the brief illustrates how a major defense contractor leveraged this platform to validate transmit/receive (T/R) modules for advanced radar systems. Their workflow required precise power sequencing, inrush capture, and fault-condition replication across chip-level components, subassemblies, and kilowatt-class radar units. Keysight’s integrated solution allowed the team to evaluate T/R modules using realistic DC-rail disturbances, voltage dropouts, surges, and low-frequency noise. Built-in protection features such as broken-sense-line detection, disconnect relays, and smart triggering safeguarded valuable hardware during repeated transient testing. The customer concluded that the platform eliminated months of system-integration work, with their field engineer stating that Keysight “hit it out of the park.”
By consolidating power sourcing, protection, measurement, and transient generation, Keysight reduces system complexity and accelerates the qualification workflow for avionics electronics. Test engineers benefit from faster setup, safer operation, deeper visibility into DUT behavior, and greater repeatability in long-duration mission profiles. The platform supports testing across chip-level avionics modules, line-replaceable units (LRUs), and high-power loads, offering scalability for both development and production environments.
In summary, Keysight’s ATE system power supplies deliver the precision, protection, and realism needed for next-generation avionics validation. Through high-speed sourcing, advanced transient capability, automated sequencing, synchronized measurement, and continuous event logging, the platform enables aerospace and defense organizations to qualify avionics systems with confidence—and without compromise.
Können wir Ihnen behilflich sein?