Technical Overviews
Introduction
Keysight Technologies’ Modulation Lab Series utilizes PathWave design software to help students develop an understanding of:
• Modulation schemes from a system level
• Modeling and simulating a communication system using PathWave System Design
Software Versions
The workspaces in these lab series were developed in Keysight PathWave System Design 2022.
Technical Sales and Support
PathWave System Design Technical Support https://bit.ly/3iK4Sr8
PathWave System Design Sales Support <https://bit.ly/3qThzTm>
Background for Students
In this set of exercises, you will create a variety of signals and visualize them in both the time and frequency domain using Keysight PathWave System Design, also known as SystemVue. A common SystemVue workspace is used for all the exercises. This is conceptually similar to a laboratory workbench comprised of a signal generator (the source) and signal analyzers (the sinks). The latter includes a time domain data sink which can be thought of as an oscilloscope and a frequency domain sink which is similar to a spectrum analyzer.
To begin with the exercises, it is assumed that you have a PC or laptop on which the suitable software has been installed.
Prerequisites
Students who are unfamiliar with any of the above aspects of SystemVue should take advantage of the on-line resources provided in Table 1 — a Keysight account might be required.
Table 1. An overview of on-line training resources.
Resource |
Description |
On-line link |
SystemVue video library available |
A collection of SystemVue instructional videos presented by Keysight Technologies |
|
Learn SystemVue in 5 mins |
A collection of SystemVue instructional videos presented by Anurag Bhargava Tutorial-1: What is Pathwave System Design (SystemVue) Tutorial-2: Understanding SystemVue Design Environment Tutorial-3: Getting Started with Data Flow Simulation in SystemVue Tutorial-4: Working with Graphs in SystemVue |
Blog: http://abhargava.wordpress.com T1: T2: T3: T4: |
Digital Modulation in Communication Systems |
Understand concepts of digital modulation and learn new digital modulation techniques in communication systems to make informed decisions to optimize your systems. |
|
Spectrum Analysis Basics (App Note 150) |
Spectrum Analysis Basics teaches the fundamentals of spectrum analyzers and spectrum analysis including the latest advances in spectrum analyzer capabilities. |
|
Signal Analyzer Fundamentals (What the RF) |
This course covers when and how to use different applications and capabilities of signal/spectrum analyzers to make various RF measurements. |
Topics Covered
This section is from Keysight’s Virtual Lab Program app note entitled ‘AM Waveforms’, with document number 3121-1266.EN. You can download the lab at https://connectlp.keysight.com/pathwave-systemdesign-virtual-labs.
Wireless communication and modulation
In simple terms, it could be said that radio frequency, microwave, millimeter-wave and sub-THz-wave communication systems all rely on the following fundamental principles:
• an electromagnetic (EM) carrier wave—in essence a sinewave—can transfer energy from a transmitter to a receiver without using wires (hence the term “wireless”); and
• a modulated carrier can be used to transfer information. In other words, by continually altering or modulating the characteristics of a sinusoid, we can use it to transfer information wirelessly.
What are you looking for?