6G Research | Cell Phone Tower 6G Networks

How 6G Research Will Revolutionize Mobile Experiences


Key takeaways:

By 2030, 6G is expected to be commercially available, revolutionizing connectivity with lightning-fast speeds, unprecedented bandwidths, and ultra-low latencies. It will transform various sectors, including telecommunications, manufacturing, healthcare, transportation, and entertainment.

In this article, get a glimpse of the 6G world coming to us over the next decade, and explore the 6G research initiatives that are enabling these next-generation capabilities.

What are the anticipated use cases and applications driving 6G research?

6G research | Illustration of Network Phone Grid | International Mobile Telecommunications 2030

In its International MobileTelecommunications 2030 (IMT-2030) initiative, the International Telecommunications Union (ITU) has laid out its vision for the sixth generation of wireless communications (6G) that will be available commercially starting around 2030.

At the same time, several industry groups have also published their 6G visions, including the Next GenerationMobile Networks Alliance (NGMN), the 6G Flagship, and the Next G Alliance.

The use cases and applications for next-generation communication technologies envisioned by these organizations are summarized below.

Ubiquitous connectivity

Under 6G, improved inclusivity and bridging of the digital divide are pivotal social objectives. Voice, video, and broadband services will be available even in remote areas and disaster zones through advances beyond 5G, such as better non-terrestrial networks, airborne and space-borne base station swarms, and mesh access networks.

Immersive personal digital experiences

Network bandwidths of 50-200 gigabits per second (Gbps) are expected, perhaps even one terabit per second (Tbps). With per-device throughputs of 300-500 megabits per second (Mbps) and microsecond latencies, users will enjoy rich communication and digital experiences through immersive high-resolution video calls, extended reality displays, and remote telepresence through multi-sensory and holographic interfaces.

Joint communications and sensing

The sub-terahertz frequencies being considered under 6G will enable combining communication signals with waveforms that resemble those of imaging radars. The same antennas, transceivers, and spectrum can be reused for both communications and sensing, enabling use cases like using smartphones for autonomous driving or for detecting people in low-visibility rescue missions.

Automobiles

Automobile companies are actively researching and prototyping the use of6G technologies for improved autonomous driving systems, real-time data processing, vehicle-to-everything communication, and advanced sensing capabilities.

Additionally, thanks to their reliability, time-sensitive networking features, and ultra-low latencies, 6G wireless networks are being considered as replacements for existing wired automotive networks. This will also reduce vehicle weights and improve sustainability through higher fuel efficiency.

Industrial-scale communications

Expect widespread public and private networks with extensive use of internet-of-things (IoT) devices for smart cities, agriculture, transportation, energy grids, and environmental monitoring. This will be possible due to high connection densities of 1 million to 100 million devices per square kilometer (km), high reliability, adaptive data rates, low power consumption, extended coverage, and high security.

6G-networked robots and automated vehicles will be extensively used in factories, warehouses, and logistics.

Precise positioning

Indoor and outdoor positioning with accuracies of 1-10 centimeters (cm) will enable precise object and presence detection, navigation, imaging​, and mapping.

Sustainability

The research and development into 6G networks explicitly aim for sustainability goals like high energy efficiency, low carbon footprint, and low emissions in telecom infrastructure as well as all the other industries they bolster, like manufacturing, automotive, and farming.

What are the key objectives and goals of current 6G research?

To realize the use cases listed earlier, some of the key objectives of 6G research include:

Other objectives include high reliability, coverage, security, resilience, and interoperability.

What technologies and innovations are being explored in 6G research?

Keysight 6G sub-terahertz test setup | Image of 6G research Equipment

Fig 1. Keysight 6G sub-terahertz test setup

The 6G objectives call for technical innovations at every level. We outline some of these research areas in the sections below.

Radio access network (RAN) innovations

Better efficiency, enhanced connectivity, and sustainability are sought through research projects like:

System architecture improvements

The system and network architecture research covers:

Operations and services

The operational and service enablement innovations include:

Sustainability and security innovations are addressed in other sections below.

How is 6G research studying the use of artificial intelligence and machine learning?

All 6G stakeholders envision extensive use of machine learning (ML), deep learning (DL), and artificial intelligence (AI) techniques at all levels in 6G systems. Their uses in the following areas are being researched:

What security and privacy aspects are being considered in 6G research?

Security and privacy are major challenges due to the expanded set of use cases brought by ubiquitous mobile communications. The aspects being researched include:

How does 6G research address sustainability and environmental impacts?

With policies like the European Green Deal getting legislated to tackle climate change, the 6G ecosystem has proactively set sustainability as a key goal of 6G. The IMT-2030 addresses environmental, social, and economic sustainability. It supports the United Nations' Sustainable Development Goals and the Paris Agreement.

Research in these areas includes:

What are some challenges in 6G research?

6G Research Software | Over-The-Air Measurement Results at 310 Ghz

Fig 2. Over-the-air measurement results at 310 GHz

Some of the challenges of these new technologies are:

What is the state of 6G collaborations and standardization?

6G standardization roadmap Flow and Timeline | ITU IMT-2030

Fig 3. The 6G standardization roadmap

The 6G standardization roadmap has not yet started. As of March 2024, the ITU has published its IMT-2030 vision for 6G.

Guided by its goals, several industry and academic groups have set up alliances for researching and prototyping new technologies as well as enhancements for 6G. Such groups include:

These groups will send their technical proposals for 6G to the ITU around 2027.

The ITU's expert groups will review their proposals and select the ones that are best aligned with its 6G vision.

By then, the 3rd Generation Partnership Project (3GPP), which develops the official standards, will have published its Release 19 and Release 20 specifications for 5G-Advanced and is expected to work on the6G standards as part of Release 21, which will be published by 2030.

Keysight's 6G offerings

6G research testbed | Keysight's 6G offerings Flow

Fig 4. 6G research testbed

Keysight is a key member of the above alliances and the preferred test and measurement partner of major telecom vendors and research groups. Our 6G research includes:

The state-of-the-art equipment and software used in this research, and available to clients and partners, include:

Designing a new digital world with 6G research

In this article, we explored the goals and directions of current 6G research initiatives.

Keysight's unparalleled expertise in high-frequency radio signals makes us a natural partner of choice for network equipment vendors and research groups working on 6G.

Contact us for deep insights into how your teams can streamline your 6G research using our equipment.

limit
3