Creating safe and robust autonomous driving (AD) systems is complex. Autonomous vehicles (AVs) have hundreds of sensors needing to work with one another inside the car and with other smart vehicles. The software algorithms enabling AD features will ultimately need to synthesize all the information collected from these sensors to ensure the vehicle responds appropriately. These algorithms require testing against millions of complex scenes covering various driving scenarios. Explore the Keysight radar scene emulator's three main differentiators – extended object emulation, minimum distance, and wide FOV with many objects.