您希望搜索哪方面的内容?
AXIe 机箱固化软件
根据需要更新的元器件类型,更新可能需要 60 分钟完成。在更新过程中,安装在机箱中的仪器模块取消激活 ATCA 服务状态,并且可以停用,以便降低功耗。机箱风扇速度可能在更新过程中发生变化。更新结束后,通过接通和断开机箱电源以完成安装。
发布日期 | 版本 | 版本说明 |
---|---|---|
2024-02-16 | 1.4.0 and 2.2.0 | See below. Version 1.4.0 is to be used with ESM M9505-00132, M9505-00232 or older only. Version 2.2.0 is to be used with ESM M9505-00133, M9505-00233 or greater only. |
发布日期 | 版本 |
---|---|
2024-02-16 | 1.4.0 and 2.2.0 |
版本说明 |
---|
See below. Version 1.4.0 is to be used with ESM M9505-00132, M9505-00232 or older only. Version 2.2.0 is to be used with ESM M9505-00133, M9505-00233 or greater only. |
Chassis firmware 1.4.0 contains:
- For use with ESM M9505-00132, M9505-00232, or older only. DO NOT upgrade to this FW version if you are using ESM M9505-00133, M9505-00233 or greater.
- Support M9502-00019 and M9505-00019 fan assemblies.
- Improve fan algorithm to limit fan speed in high CPU usage applications.
Chassis firmware 2.2.0 contains:
- For use with ESM M9505-00133, M9505-00233 or greater only. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
- Support M9502-00019 and M9505-00019 fan assemblies.
- Improve fan algorithm to limit fan speed in high CPU usage applications.
- Add delay feature for PCIe Upstream Connection.
如何下载
- Click the download button and save the file to your PC
如何安装
颁发许可证
- Does Not Require a License
Installs on: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 8.1
- Windows 10
前提要求
- Version 1.4.0: For use with ESM M9505-00132, M9505-00232, or older only. DO NOT upgrade to this FW version if you are using ESM M9505-00133, M9505-00233 or greater.
- Version 2.2.0: For use with ESM M9505-00133, M9505-00233 or greater only. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
支持的仪器
- M9502A, M9505A
Chassis firmware 1.3.46 contains:
- For use with ESM M9505-00132, M9505-00232, or older only. DO NOT upgrade to this FW version if you are using ESM M9505-00133, M9505-00233 or greater.
- Resolve chassis FRU issue with checksum error during firmware bootup showing behaviors of ESM status LED always flashing green and not enumerating installed modules.
- Firmware update to 1.3.46 or later is recommended if the ESM is moved to a different chassis.
Chassis firmware 2.1.6 contains:
- For use with ESM M9505-00133, M9505-00233 or greater only. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
- Resolve chassis FRU issue causes modules unable to enumerate when using with USB ESM.
- Resolve unable to set fan speed issue when using with non_USB ESM
如何下载
- Click the download button and save the file to your PC
如何安装
颁发许可证
- Does Not Require a License
Installs on: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 8.1
- Windows 10
前提要求
- Version 1.3.46: For use with ESM M9505-00132, M9505-00232, or older only. DO NOT upgrade to this FW version if you are using ESM M9505-00133, M9505-00233 or greater.
- Version 2.1.6: For use with ESM M9505-00133, M9505-00233 or greater only. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
支持的仪器
- M9502A, M9505A
Chassis firmware 1.3.46 contains:
- For use with ESM M9505-00132, M9505-00232, or older only. DO NOT upgrade to this FW version if you are using ESM M9505-00133, M9505-00233 or greater.
- Resolve chassis FRU issue with checksum error during firmware bootup showing behaviors of ESM status LED always flashing green and not enumerating installed modules.
- Firmware update to 1.3.46 or later is recommended if the ESM is moved to a different chassis.
Chassis firmware 2.1.5 contains:
- For use with ESM M9505-00133, M9505-00233 or greater only. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
- Allow ESM M9505-00133, M9505-00233 or greater to work with chassis serial number TW61130000 or below.
- Resolve chassis FRU issue with checksum error during firmware bootup showing behaviors of ESM status LED always flashing green and not enumerating installed modules.
- Firmware update to 2.1.5 or later is recommended if the ESM is moved to a different chassis.
如何下载
- Click the download button and save the file to your PC
如何安装
颁发许可证
- Does Not Require a License
Installs on: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 8.1
- Windows 10
前提要求
- Version 1.3.46: For use with ESM M9505-00132, M9505-00232, or older only. DO NOT upgrade to this FW version if you are using ESM M9505-00133, M9505-00233 or greater.
- Version 2.1.5: For use with ESM M9505-00133, M9505-00233 or greater only. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
支持的仪器
- M9502A, M9505A
Chassis firmware 2.1.4 contains:
- Initial release to support newer version of ESMs used together with chassis serial number TW61130001 or greater. This FW can only be used with ESM M9505-00133, M9505-00233, or greater. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
- Chassis serial number TW61130000 or below with ESM M9505-00132, M9505-00232, or older should only use FW version 1.3.45. This FW can only be used with ESM M9505-00133, M9505-00233, or greater. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232, or older.
- Repair issue with hotplug of the USB cable for ESM M9505-00233 or greater.
- Add new "Publish Address" ipmi command for ESM M9505-00233 or greater. This allows the DDS modules such as U4421A and U4431A to work in chassis with serial number TW61130001 or greater.
如何安装
颁发许可证
- Does Not Require a License
Installs on: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 8.1
- Windows 10
前提要求
- For use with chassis serial number TW61130001 or greater and with ESM M9505-00133, M9505-00233 or greater only. DO NOT upgrade to this FW version if you are using ESM M9505-00132, M9505-00232 or older.
支持的仪器
- M9502A, M9505A
Chassis firmware 1.3.45 will:
- Rebrand the Chassis Web Interface from “Agilent” to “Keysight”.
- Repair Health tab on M950xA Web Interface showed incorrect values at Sensor readings.
如何下载
- Click the download button and save the file to your PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
Chassis firmware 1.3.44 will:
- Update the shelf manager to firmware 1.44.
- Repair an intermittent issue where the chassis is unable to communicate with modules after a boot up if this firmware is combined with chassis drivers 1.4.4.1 or later. This will support obtaining chassis IP address through PCIe switch register instead of using LxiMdnsResponder to resolve the issue.
如何下载
- Click the download button and save the file to your PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
Fixed 3 problems that caused:
- embedded controller M9537A to fail to detect some AXIe modules.
- embedded controller M9037A to fail to establish a PCIe link to the M9502A/M9505A when using some Y1202A PCIe cables.
-
the minimum fan level to not be enforced during startup after the dynamic minimum fan level was set in the previous session.
如何下载
- Click the download button and save the file to your PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
安装到: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 8.1
- Windows 10
前提要求
- No specific prerequisites
支持的仪器
- M9502A, M9505A
如何下载
Click the download button and save the file to your PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
如何下载
1. 点击下载按钮
2. 将 .zip 文件保存到主机(c:/tmp)
3. 将程序包解压到 PC 中
如何安装
颁发许可证
- 不要求具有许可证
支持文档
安装到: Instrument
操作系统
- Windows 7
- Windows XP
前提要求
升级 AXIe 机箱固化软件要求 PC 主机上装有 Agilent IO 程序库。如果尚未安装,您可以从以下网址下载: http://www.agilent.com/find/iosuite。
支持的仪器
- M9502A, M9505A
如何下载
- Click Download button
- Save .zip file to host computer (c:/tmp)
- Unzip the package to your PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
安装到: Instrument
操作系统
- Windows 7
- Windows XP
前提要求
- To upgrade the AXIe chassis firmware, you must have Agilent IO Libraries installed on the host PC. If it is not already installed, you can download it here: http://www.agilent.com/find/iosuite.
支持的仪器
- M9502A, M9505A
如何下载
- Click Download button
- Save .zip file to host computer (c:/tmp)
- Unzip the package to your PC
如何安装
- Refer to Firmware Update Guide (included in .zip file)
颁发许可证
- 不要求具有许可证
支持文档
安装到: Instrument
操作系统
- Windows 7
- Windows XP
前提要求
- To upgrade the AXIe chassis firmware, you must have Agilent IO Libraries installed on the host PC. If it is not already installed, you can download it here: http://www.agilent.com/find/iosuite
支持的仪器
- M9502A, M9505A
如何下载
- Click Download button
- Save .zip file to host computer (c:/tmp)
- Unzip the package to your PC
如何安装
- Refer to Firmware Update Guide (included in .zip file)
颁发许可证
- 不要求具有许可证
支持文档
安装到: Instrument
操作系统
- Windows 7
- Windows XP
前提要求
- To upgrade the AXIe chassis firmware, you must have Agilent IO Libraries installed on the host PC. If it is not already installed, you can download it here: http://www.agilent.com/find/iosuite
支持的仪器
- M9502A, M9505A