Revision String Numbering Format
The chassis firmware revision string is organized in the following format:
Where...
- F2AX Identifies an M9502A 2 slot AXIe chassis
- F5AX Identifies an M9505A 5 slot AXIe chassis
- F2A Identifies an older AMP 2 slot style chassis (which is not supported by this update procedure)
-
< major > Identifies the major release number -
< minor > Identifies the minor release number -
< build > Identifies a build number
-
< xxxx > is a hexadecimal value identifying the backplane fan firmware revision.
-
is a hexadecimal value for the specific firmware component. The actual content of these components is for Keysight internal use only.
A firmware revision example:
F2AX-1.3.37-0107-A002e-B12062214-CA1.0-DA1.0-E1.3
This example identifies...
- M9502A AXIe 2 slot chassis using chassis firmware revision 1.3.37.
- The backplane revision number is 0107.
- Component A is at revision 002e, component CA is at revision 1.0, component DA is at 1.0, and component E is at 1.3.
- The actual content of these components is for Keysight internal use only.