What are you looking for?
BenchVue Basic Offline Installer Download
This is the offline installer for Keysight BenchVue Basic (Standalone App and Platform/Non-Standalone App).
For your convenience, we provide separate installers tailored to online and offline installation scenarios. Whenever possible, we highly recommend opting for the online installer for improved efficiency and reduced bandwidth usage. You can easily access the online installer at www.keysight.com/find/BVBasic.
The offline installer serves as a solution for situations where internet connectivity is unavailable. Please note that it is notably larger in size and may not include the most up-to-date features, bug fixes, or security patches.
One of the key advantages of BenchVue Basic is that it requires no licensing, ensuring easy and immediate use of the BenchVue software to make the most of your instrument.
It is important to note that BenchVue Basic Apps do not include technical support. If you require technical support or seek access to the most current software version, we recommend exploring the licensed version of the app.
| Release Date | Version | Version Description |
|---|---|---|
| 2023-12-22 | 2023.2 | This version provides updated offline installers for BenchVue Basic Standalone apps and Platform/Non-standalone apps. Further details of app versioning are available in the release notes below. |
| Release Date | Version |
|---|---|
| 2023-12-22 | 2023.2 |
| Version Description |
|---|
| This version provides updated offline installers for BenchVue Basic Standalone apps and Platform/Non-standalone apps. Further details of app versioning are available in the release notes below. |
How to Download
- Click the Download button to initiate the download.
- Save the ZIP file to your hard drive. If the download doesn't start correctly, consider disabling your browser's pop-up blocker.
How to Install
- Locate the downloaded ZIP file, right-click on it, and select Extract All. Follow the on-screen instructions to extract the files, which will be placed in the same directory as the ZIP file.
- Navigate to the directory where the extracted files are located, then double-click on the installer to commence the software installation.
- For detailed installation guidance, refer to the ReadMe file named ReadMe_First.txt included with the download.
Licensing
- No cost, Perpetual, Floating (unlimited copies) license (no activation required)
Supporting Documentation
Installs On
- PC
Operating System
- Microsoft Windows 10 (64-bit, version 1809 or later)
Prerequisites
- Intel Core i5 (or equivalent) with 8 GB RAM or better
- 20 GB free hard disk space
- Display resolution 1920x1080 recommended
Supported Instruments
How to Download
- Click the Download button to initiate the download.
- Save the ZIP file to your hard drive. If the download doesn't start correctly, consider disabling your browser's pop-up blocker.
How to Install
- Locate the downloaded ZIP file, right-click on it, and select Extract All. Follow the on-screen instructions to extract the files, which will be placed in the same directory as the ZIP file.
- Navigate to the directory where the extracted files are located, then double-click on the installer to commence the software installation.
- For detailed installation guidance, refer to the ReadMe file named ReadMe_First.txt included with the download.
Licensing
- Does not require a License
Supporting Documentation
Installs On
- PC
Operating System
- Microsoft Windows 10 (64-bit, version 1809 or later)
Prerequisites
- Intel Core i5 (or equivalent) with 8 GB RAM or better
- 20 GB free hard disk space
- Display resolution 1920x1080 recommended