Data Sheets
System Description
Keysight's threat simulator is a fully integrated system. A single rack provides 2 channels (1 channel x 4 ports and 1 channel x 8 ports). Addition of a second identical rack expands the system to 4 channels (2 channels x 4 ports and 2 channels x 8 ports). All ports are aligned in amplitude, phase and time using the Z2098B-186 calibration system.
Simulation Capability (Z2098B-185)
The Keysight threat simulator provides complete measurement capability for:
Calibration Methods (Z2098B-186)
The Keysight calibration system provides calibration and verification of the threat simulator by aligning amplitude, phase and time between the source rack and the System Under Test (SUT).
Mean Time To Repair (MTTR)
CalPod/Coupler Module In-Situ Calibration and Verification Concept
CalPods provide a way to quickly and easily refresh a network analyzer calibration, at the push of a button and without
removing the SUT or re-connecting standards. This capability is used to enhance the accuracy of the source calibration.
The VNA is used to monitor the coupled source signal close to the SUT. Using CalPods, the VNA calibration can be refreshed as needed prior to a source rack amplitude and phase calibration to provide the best possible performance. With the CalPods in place near the SUT inputs, the entire source calibration can be calibrated or verified while the SUT remains attached to the source. Support to initialize the CalPods and characterize the couplers is provided by the System Level Calibration (SLC) software included with the Z2098B-186 calibration rack.
What are you looking for?