Technical Overviews
Testing balanced devices using true-mode drive
True-mode stimulus
By using a dual-source 4-port network analyzer, we are able to accurately control both internal sources simultaneously and therefore, to correct for the phase and amplitude differences at every frequency point for each true-mode measurement, at the reference plane of the device-under-test (DUT). This way, we can set the phase difference to zero for common-mode stimulus, or to 180 degrees for differential-mode stimulus, while maintaining the same amplitude. In addition, we provide a mode where the user can set the phase difference of a continuous-wave (CW) to any arbitrary value between 0 and 180, as well as setting the amplitude difference to an arbitrary value. This allows for imbalanced stimulus to perform stress tests on the DUT as needed.
Fully match-corrected calibrated differential sources
The match-corrected source calibration is the calibration of the waves so that the actual waveform at the reference plane of the DUT is modified to maintain a precise differential- or common-mode drive, taking into account the mis-match of the DUT and the test system. This modification does not require any extra work from the user, but it does require the network analyzer to make two measurements at each frequency point. All the necessary steps are managed and executed by the True-Mode Stimulus Application (TMSA). At each frequency point, the application will:
Fully error-corrected measurements
After the fully-calibrated true-mode drive signal is applied, all the scattered waves (S-parameters) from the DUT are measured, and the effects of the re-reflections from the network analyzer are removed through a modified full 4-port error-correction. A modification is required because, unlike the single ended measurement, only two of the ports are terminated during a measurement, the other two ports are being driven by the true-mode signal. Once again, all necessary steps are managed and executed by TMSA with no added work required from the user. Because error correction is possible by applying standard 4- or 3-port calibration techniques and then modifying the error-term matrix, the error-correction process is simply to perform a full 4- or 3-port single-ended calibration (depending on the topology being measured), using either an Electronic Calibration (ECal) module or mechanical calibration kit, before launching the true-mode stimulus application. An ECal module, either 2- or 4-port, would provide the fastest and most convenient approach.
Measurement process overview
Whether you are measuring a 4-port device, with balanced-input and balanced- output (BAL-BAL), or a 3-port device, with one port single-ended and one port balanced (SE-BAL), a dual-source 4-port network analyzer is required for true-mode stimulus. To obtain true-mode stimulus parameters, the user only needs to add one more step to the measurement process and that is to activate TMSA. In general, the following steps do apply:
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.
What are you looking for?