Advanced Calibration Techniques to improve Extinction Ratio Measurement in DCA-X and DCA-M

Application Notes

Extinction Ratio Measurement Fundamentals

Extinction ratio (ER) is a measurement that represents how well available laser power is converted to modulation power. Mathematically it is the ratio of the logic ‘1’ level to the logic ‘0’ level. If very little power is used to transmit a ‘0’ level relative to the ‘1’ level power, the ER will be high, an indication that the laser power is efficiently being used as modulation power. For PAM4 (Pulse Amplitude Modulation 4-level) signals the definition is similar, but the ratio is composed of the ‘3’ and ‘0’ levels. ER is a primary specification for every transmitter used in direct detection communication systems. Long span systems place a higher importance on ER and historically have required high values. Shorter span systems place less stringent requirements on ER. 

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.