E16-5jl02
CVSS:
8.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2016
Description
This strike exploits a use after free vulnerability in Microsoft Internet Explorer and Edge Browsers. Specifically, if a font element's lang attribute is set to a string, and then its node value is set to null, the string is freed. Later a call to reference this lang attribute will result in a user after free condition. An attacker can use this attack to disclose memory information that can potentially lead to an ASLR bypass.