Adobe Flash Player MovieClip Use After Free Vulnerability

Strike ID:
E15-6yi01
CVSS:
10.0 (AV:N/AC:L/Au:N/C:C/I:C/A:C)
False Positive:
f
Variants:
2
Year:
2015

Description

This strike exploits a remote code execution vulnerability in Adobe Flash Player. The vulnerability is due to a use after free while calling MovieClip.scrollRect in AS2. An attacker can entice a target to open a specially crafted flash file to trigger the vulnerability. Successful exploitation may result in execution of arbitrary code or abnormal termination of the flash process.

CVE

References

Bid