OpenEMR multiple SQL Injection

Strike ID:
E18-0q4i1
CVSS:
8.8 CVSS:3.0/AV:N/AC:L/PR:L/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
4
Year:
2018

Description

This strike exploits a SQL injection in OpenEMR open-source project. The vulnerability is due to insufficient user input sanitization passed through the URI, addressing various PHP scripts. A specially crafted HTTP GET request can cause a SQLi in the context of the database user.

CVE

References