TerraMaster NAS Username System Command Injection

Strike ID:
E20-5k623
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2018

Description

This strike exploits a vulnerability in the TerraMaster NAS device. This device allows for the option to pass command line arguments to the system during the creation of a user but does not properly validate the arguments passed. It is possible to execute system commands as a root user on a vulnerable device.

CVE

References