Foxit Studio Photo PSD File ImageResourceBlocks Out of Bounds Read

Strike ID:
E20-159r1
CVSS:
4.3 CVSS:3.1/AV:N/AC:L/PR:N/UI:R/S:U/C:L/I:N/A:N
False Positive:
f
Variants:
1
Year:
2020

Description

This strike exploits an out-of-bounds read vulnerability in Foxit Studio Photo versions up to 3.6.6.916. The vulnerability is due to the lack of proper validation of user-supplied data, which can result in a read past the end of an allocated structure when handling PSD files. An attacker could exploit this vulnerability by creating a specially crafted PSD file and entice a user to open it. Successful exploitation could lead to information disclosure.

CVE

Metasploit

Zdi