E17-0hv81
CVSS:
7.5 CVSS:3.0/AV:N/AC:H/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
128
Year:
2017
Description
This strike exploits a vulnerability in Microsoft Edge. Specifically, the Javascript Chakra engine assumes that the specified array will be a float array, however, it is possible to modify this type with the valueOf handler, which will result in type confusion. This can cause a denial of service in the browser or potentially allow for remote code execution to occur.
CVE
https://code.google.com/p/google-security-research/issues/detail?id=1290