Landslide AI Agent

Solution Briefs

Landslide AI Agent introduces a new approach to mobile network testing by embedding agentic AI directly into the validationworkflow, addressing the growing complexity of 5G Standalone networks, cloud-native architectures, and emerging 6G environments. As service providers and infrastructure teams manage increasingly dynamic, multi-vendor ecosystems with rapid software release cycles and expanding security demands, traditional testing and troubleshooting methods are becoming unsustainable. Engineers are faced with overwhelming volumes of data, including logs, packet captures, configuration files, and standards documentation, while also being expected to accelerate validation timelines and maintain high service reliability. Landslide AI Agent is designed to meet these challenges by transforming how testing, analysis, and knowledge access are performed within the Landslide 5G Core Test Solution.

 

At its core, Landslide AI Agent is an embedded, on-premises AI solution purpose-built for mobile network validation and assurance. It combines structured domain knowledge with a multi-agent AI architecture to deliver intelligent automation across three primary functions: contextual knowledge retrieval, automated test case generation, and accelerated root cause analysis. Unlike general-purpose AI tools, Landslide AI Agent is specifically trained on telecom validation workflows and aligned with 3GPP standards, protocol behavior, and real-world troubleshooting practices. This ensures that outputs are not only fast but also accurate, explainable, and grounded in domain expertise.

 

A key differentiator of Landslide AI Agent is its multi-agent architecture, which integrates a domain-specific retrieval-augmented generation knowledge graph, deterministic rule engines, and fine-tuned local language models. This hybrid approach minimizes the risks commonly associated with large language models, such as hallucinations, by anchoring analysis in verified data and predefined rules. The language model component is primarily used for natural language interaction, enabling engineers to query the system conversationally while maintaining confidence in the technical validity of responses. Additional specialized agents handle tasks such as packet capture analysis, configuration parsing, anomaly detection, and prioritization, allowing Landslide AI Agent to deliver comprehensive insights across complex datasets.

 

Landslide AI Agent is tightly integrated into the Landslide platform, providing engineers with real-time, context-aware assistance during test execution. Users can interact with the system through a conversational interface that understands the current test environment, including active scenarios, detected anomalies, and system state. When issues arise, Landslide AI Agent automatically correlates data from multiple sources, analyzes behavior against standards and historical patterns, and generates prioritized root cause explanations. This dramatically reduces the time and effort required for troubleshooting. Landslide AI Agent has demonstrated the ability to reduce a seven-week root cause analysis process to just minutes, highlighting its potential to transform operational efficiency.

 

Beyond troubleshooting, Landslide AI Agent significantly enhances test development workflows. Engineers can use natural language prompts to generate new test cases, validate scripts before execution, and modify existing scenarios. This reduces the reliance on deep protocol expertise for test creation and accelerates onboarding for new team members. By automating routine and complex tasks, Landslide AI Agent enables organizations to expand test coverage without increasing headcount, while also freeing experienced engineers to focus on higher-value activities.

 

Security and data control are central to Landslide AI Agent’s design. The solution is deployed on-premises as part of the Landslide platform, ensuring that all data, including logs, KPIs, and proprietary knowledge, remains within the customer’s environment. This is critical for telecom operators and enterprises that must adhere to strict data governance and security requirements. The architecture requires only local compute resources, such as GPU-enabled servers, and eliminates dependence on external cloud services.

 

Landslide AI Agent also supports a broader evolution toward automated, continuous validation workflows. While it initially operates with human-in-the-loop verification, its roadmap includes integration into CI/CD pipelines, enabling scalable and automated root cause analysis and test execution. This progression aligns with the industry shift toward continuous testing and assurance, particularly as networks become more software-driven and distributed. Future integration with platforms such as Velocity and VisionWorks further extends Landslide AI Agent’s capabilities into end-to-end, AI-driven validation ecosystems.

 

The operational impact of Landslide AI Agent is significant. It reduces troubleshooting cycles from weeks to minutes, improves consistency and determinism in analysis, and alleviates cognitive overload for domain experts. By enabling faster iteration and deeper validation coverage, it helps organizations accelerate time to deployment while maintaining high quality and reliability standards. Rather than reducing testing efforts, Landslide AI Agent enables more comprehensive and efficient testing, supporting the increasing demands of modern network environments.

 

As the industry moves toward AI-native 6G architectures, the need for intelligent, scalable validation solutions will only grow. Landslide AI Agent represents a foundational step in this direction, embedding intelligence directly into the testing process and enabling a shift from reactive troubleshooting to proactive validation. By combining decades of domain expertise with advanced AI techniques, it delivers a smarter, more efficient approach to network assurance, positioning organizations to meet the challenges of next-generation connectivity with confidence.