The Citizen Developer Movement

eBooks

Overview

 

The citizen developer movement is helping businesses develop automation solutions faster so they can power productivity and drive efficiency. But while no-code low-code platforms provide the tools to create the apps, how are businesses managing the quality and maintenance requirements of the solutions they develop? This playbook explores the rise of the citizen developer movement and looks at how to embrace the opportunities without compromising on quality.

 

Introduction

 

There is no question of the value of citizen developers – but like any growing movement, difficulties are emerging as it matures. Chief amongst these is how to maintain citizen developed apps and drive quality. Because while there is a robust QA culture – and the tools to match – in the world of traditionally developed apps, the same cannot be said of citizen developed apps.

 

This playbook explores the rise of the citizen developer movement, the value it brings and the problems it presents. It then suggests a solution that allows organizations to benefit from the best of both worlds.