The Power of Proactive Active Assurance Use Cases

White Papers

We need a fundamental shift in our approach to assuring the network. The network is moving to the cloud. Functions are now virtualized. And next-gen networks are too dynamic for manual troubleshooting to handle. There is a compelling argument for employing Active Assurance in tandem with Passive Assurance. As 5G and SD-WAN drive us to adopt virtualization, Active Assurance will be a critical enabler of the automation needed to successfully ensure differentiated performance and quality for these next-gen services.