How to Setup Parameterization

How-To Videos

This video describes the basics of performing parameterization on Windows OS Application and Linux OS Terminal. Keysight PathWave Instrument RPA parameterization feature enables the setting of input variable as a parameter. The conditions and behavior of the parameter can subsequently be edited on Visual Script Editor. Parameterization is helpful to drive repetitive test which changes specific parameters many times, although it supports the same test procedure.