Cyber Resilience – Healthcare’s Most Important Asset

White Papers

What Is Cyber Resilience?

It’s no longer a case of if your hospital, clinic, insurance company, or other healthcare-related entity will be attacked — it’s a question as to when. As a reference point, a Black Book Market Research report showed that over 93% of healthcare organizations experienced one data breach between 2016 and late 2019 and 57% of organizations had over five breaches during that timeframe.

Organizations should be especially concerned about security breaches and ransomware in the current geopolitical climate. Attacks could come at any time. However, there is something you can do to mitigate breach risk. By adopting a resilient security architecture approach, the “time to observance” and “time to remediation” can be reduced. This is where cyber resilience comes into play. Cyber resilience is a strategy designed to help you reduce the cost and risk associated with a data breach.

A resilient approach allows you to:

  • Strengthen your capabilities to defend against attacks
  • Maximize your ability to rebound from an attack
  • Minimize the severity and cost of security breaches