何をお探しですか?
Keysight Works with Qualcomm Technologies to Accelerate Small Cell Deployment Supported by 5G vRAN Architecture
Expands ecosystem to speed development of radio units (RU)
SANTA ROSA, Calif., March 2, 2020
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, announced that Qualcomm Technologies, Inc., a wholly owned subsidiary of Qualcomm Incorporated, is working with the company to accelerate small cell deployment supported by 5G virtualized radio access network (vRAN) architecture.
Mobile operators are expected to increasingly deploy small cells, especially indoors, to deliver enhanced wireless services that rely on high data rates and low latencies. These services are designed to deliver improved production efficiencies in factories, greater reliability in mobile connectivity for enterprises, and uniform experiences for consumers accessing on-line gaming, live TV, as well as augmented and virtual reality applications.
Keysight's 5G Multi-Band Vector Transceiver and Qualcomm Technologies' 5G RAN solutions speed development of radio units (RU) critical to addressing a wide range of 5G use cases. Keysight's 5G Multi-Band Vector Transceiver is a PXI-based compact solution that enables automated testing of the transmitter and receiver characteristics of a 5G new radio (NR) base station, according to the 3GPP specifications. The solution accelerates verification of small cell RUs using the 5G NR capability of Qualcomm® FSM™100xx to support a smooth transition from product design to manufacturing test.
"We're pleased to work with Qualcomm Technologies to support the development of the 5G small cell industry, which is expected to grow at a 10 percent CAGR over the next five years to reach $5.2 billion by 2024, according to Mobile Experts," said Giampaolo Tardioli, vice president and general manager of Keysight's network access group. "The versatility of Keysight's 5G Multi-Band Vector Transceiver enables makers of radio units to accelerate design validation and manufacturing test in a highly automated environment."
Keysight's comprehensive 5G solution portfolio enables network equipment manufacturers (NEMs) and mobile operators to address a wide range of test, validation and optimization requirements related to the deployment of disaggregated networks using vRAN architecture and Open RAN standard interfaces. The integrated solution portfolio creates unique end-to-end performance visibility from the edge of the radio access network (RAN) to the 5G core (5GC).
"We are happy to be working closely with Keysight to serve the burgeoning 5G industry, and we aim to provide fast, enhanced mobile connectivity by improving network coverage, capacity, performance and power efficiency through our advanced 5G RAN solutions," said Puneet Sethi, senior director, product management, Qualcomm Technologies, Inc. "By working with industry-leaders like Keysight, we can quickly put cutting-edge technology in the hands of customers and help them accelerate the deployment of 5G small cells to the industry."
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $4.3B in fiscal year 2019. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Qualcomm and FSM are trademarks of Qualcomm Incorporated, registered in the United States and other countries.
Qualcomm FSM is a product of Qualcomm Technologies, Inc. and/or its subsidiaries.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Need to contact Media Relations at Keysight?