E18-0ouo1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
12
Year:
2018
Description
This strike exploits a vulnerability in Drupal Core open-source CMS. The vulnerability is due to improper validation of user-supplied data while performing server-side deserialization of PHP objects. A malicious user can exploit this vulnerability by sending multiple HTTP POST requests including serialized PHP objects. When successfuly exploited, the vulnerability results in complete compromise of the target server.