E20-5k5u1
CVSS:
7.2 CVSS:3.0/AV:N/AC:L/PR:H/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2018
Description
This strike exploits a vulnerability in the TerraMaster NAS device. This device allows for the option to pass command line arguments to the system during the creation of a user but does not properly validate the arguments passed via the groupname parameter. It is possible to execute system commands as a root user on a vulnerable device.