How to Perform Burst Power Measurement

Power Meters and Sensors
+ Power Meters and Sensors

Measure Burst RF Power Accurately

Burst power measurement in time-division multiple access (TDMA) and pulsed radio frequency systems requires isolating signal power during active transmission intervals while excluding idle periods. This is accomplished using time-gated measurement techniques, where the measurement window is precisely aligned with the burst timing of the signal. Engineers must configure gate delay, gate width, and trigger synchronization to ensure that the power sensor captures only the intended portion of the waveform. Accurate results depend on the sensor's response time, timing resolution, and the ability to repeat measurements consistently across multiple burst cycles. Any misalignment between the gate and the signal can introduce averaging errors and distort the measured power value.

The measurement setup includes an average power meter, compatible power sensors, and software capable of controlling gating parameters and automating acquisition. Multiple bursts are captured and averaged to improve measurement confidence and reduce the effects of variation between individual pulses. Engineers use data logging and visualization tools to analyze burst-to-burst stability, verify timing alignment, and observe any drift or variation over time. Proper configuration of the measurement system ensures that only the active signal energy is included in the calculation, enabling accurate and repeatable burst power measurements across a range of TDMA and pulsed signal conditions.

Accurate Burst Power Measurement Solution

Burst power measurements require instrumentation capable of accurately synchronizing measurement acquisition with the active transmission interval while providing repeatable power measurements across successive bursts. The measurement workflow begins by configuring trigger conditions and time-gating parameters, followed by synchronization between the power meter, sensor, and signal source to isolate the desired portion of each burst. The solution combines an average power meter, USB and peak-and-average power sensors, and power measurement software to automate gated acquisitions, configure timing parameters, and continuously log measurement results. Engineers can monitor burst-to-burst repeatability, compare average power across multiple acquisitions, and visualize timing alignment while exporting measurement data for further analysis or production reporting. Automated control and synchronized data acquisition simplify characterization of TDMA and pulsed radio frequency transmitters, reducing manual measurement steps while maintaining consistent and repeatable burst power results throughout design validation, troubleshooting, and functional verification workflows.

See Block Diagram of Burst Power Measurement Solution

N1913B Average Power Meter, BV0007B Power Meter Software, U2000A USB Power Sensor,  E9326A Peak and Average Power Sensor

Explore Products in Our Burst Power Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?