E18-0jw41
CVSS:
5.9 CVSS:3.0/AV:N/AC:H/PR:N/UI:N/S:U/C:N/I:N/A:H
False Positive:
f
Variants:
1
Year:
2018
Description
This strike exploits a code execution vulnerability in Squid Proxy.
The vulnerability is due to improper handling of objects in memory within the ESI and OpenSSL functionalities of the server.
By sending a crafted ESI responses to the target server, the attacker can cause denial-of-service conditions on the target proxy service.
CVE
References
Metasploit
http://www.zerodayinitiative.com/advisories/ZDI-18-309
Zdi
18-309