Cesanta Mongoose MQTT SUBSCRIBE Denial of Service

Strike ID:
E19-0di51
CVSS:
7.5 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:N/I:N/A:H
False Positive:
f
Variants:
3
Year:
2017

Description

An exploitable NULL pointer dereference vulnerability exists in the MQTT packet parsing functionality of Cesanta Mongoose. To trigger this vulnerability, an attacker must send a specially crafted MQTT SUBSCRIBE packet over the network, without a preliminary CONNECT packet. Successful exploitation results in remote code execution or denial of service conditions of the application.

CVE

References