Choose a Platform :

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2025-12-19 2026.0 See Release notes
Release Date Version
2025-12-19 2026.0
Version Description
See Release notes

Key Highlights of Keysight Stamping 2026.0

New Forming & Process Capabilities

  • Tailor Welded Blanks (TWB) definition at the blank stage with independent material and thickness zones
  • Tool scaling to compensate for springback without returning to CAD
  • Kinematic check for instant validation of tool strokes and motion sequences
  • Compensation “ignore zones” to prevent downstream operations from influencing compensated tool geometry
  • Robustness analysis via strategic integration with Return On Data (CAPY-Q.Form)

Improved User Experience

  • Complete interface redesign with a modern look & feel
  • More intuitive interaction and higher productivity
  • No workflow changes and no retraining required

Faster Turnaround Time

  • Major GUI performance improvements, enabling near-instant interaction even for large models
  • Enhanced Virtual Light Room performance for faster cosmetic defect assessment
  • New automatic PowerPoint reporting with one-click image and video export using customizable templates

Increased Predictive Confidence

  • Improved edge crack prediction with edge strain computation
  • New maximum failure risk contour to detect forming limit violations across the entire forming cycle
     

How to Download

  • Click the Download button
  • Continue to Keysight Software Manager to download Software Updates

Licensing

  • Requires a License

Operating System

  • Windows 64

Prerequisites

Downloads

Stamping 2026.0 for Windows

File Size: 5.44 GB
MD5: da649a43682a126786dd8f0a7fafdb34
Info: BM-Stamp 2026.0  for Windows including CSM Solver 46.1.0, Fit2Design 2.0.1 and Visual-Environment 24.0

How to install:
Unzip Keysight_BM-Stamp-2026.0_Windows.zip in a temporary directory and execute Keysight_BM-Stamp-2026.0_Windows_Setup.exe

CAPY-Q V2026.1 for Windows

File Size: 0.98 GB
MD5: 9878f78c7b755dda8f78172abb98100d
Info: CAPY-Q 2026.1 installer for Windows

How to install:
Execute   CAPY-Q_2026.1.0_installer.exe

We are excited to announce the release of the first industrial version of Keysight CAE Stamping, now available for download. Designed specifically for the automotive industry, BM-Stamp supports key stamping processes, including line/transfer die and hot forming.

This cutting-edge solution delivers the highest level of predictive confidence in simulation results, thanks to the advanced physics of the integrated Sheet Metal Forming (PAM-STAMP) solver, which has been industrially proven for over 25 years in the market.

What sets Keysight CAE Stamping apart is its seamless integration with a highly intuitive and user-friendly graphical interface, making it easy for every engineer to generate high-quality simulation results effortlessly.

The combination of a robust, accurate solver with an efficient graphical interface significantly reduces lead time by further minimizing risk during physical tryouts, and as such cutting down on iteration loops. This results in substantial savings in both cost and time during the crucial, high-risk stage of manufacturing.

Stamping is the perfect solution to help you optimize your stamping manufacturing processes, providing the confidence you need to succeed.

 

View more details about this release on Stamping 2025.0 Release Notes.


How to Download

  • Click the Download button
  • Continue to Keysight Software Manager to download Software Updates

Licensing

  • Requires a License

Supporting Documentation

Installs on: PC

Operating System

  • Windows 64

Prerequisites

Downloads

Stamping 2025.0 for Windows

File Size: 3.93 GB
MD5: 5032ba9fe74e654b37fad89b53e19677
Info:

BM-Stamp 2025.0  for Windows including CSM Solver 45.1.0, Fit2Design 1.1 and Visual-Environment 21.0

 

How to install:

Unzip BMStamp2025r0_Windows.zip in a temporary directory and execute BMStamp2025r0_SetupWindows.exe

Stamping 2023.6 is the latest release of Keysight CAE Automotive Stamping solution in Visual-Environment. Please refer to the release notes to know more about all the enhancements in this version


How to Download

  • Click the Download button
  • Continue to Keysight Software Manager to download Software Updates

Licensing

  • Requires a License

Supporting Documentation

Installs on: PC

Operating System

  • Windows 64

Prerequisites

Downloads

Stamping 2023.6 Solver for Windows

File Size: 857.67 MB
MD5: 1b19da90a00dc7bf3e46767c97488557
Info:

BODY MANUFACTURING STAMP 2023.6  for Windows including CSM Solver 44.2.1 and Fit2Design 1.1

BM-Stamp 2023.6 requires installation of Visual-Environment 2023.6

How to install:

Unzip BMStamp2023r6_Windows.zip in a temporary directory and execute setup.exe

BM-Stamp 2023.6 (Visual-Environment GUI 2023.6) for Windows

File Size: 3.25 GB
MD5: 42275cf38bdcc156adc1cd6d6f5e54ed
Info:

Visual-Environment for BM-Stamp 2023.6 on Windows.

How to install:

Unzip VisualEnvGui20236_Windows.zip in a temporary directory and execute setup.exe

Stamping is the latest addition to the Keysight CAE Manufacturing Suite. It has been developed to efficiently support the most common sheet metal manufacturing processes in the automotive industry (line die/transfer die, progressive die, hotforming).

Being integrated in the VISUAL platform, Keysight CAE is now offering a complete AUTOMOTIVE solution in a single environment for the chain, starting with single part manufacturing (sheet metal forming, composites, casting), continuing with the assembly of these parts into (sub-) assemblies (welding, riveting, gluing,…) and final performance testing under realistic conditions (crash, durability, ergonomics,..), taking into account dimensional and cosmetic quality at each stage.

This first release of Stamping is addressing the line die process (cold forming) and supports the user through a powerful, state-of-the-art graphical interface with many intuitive functionalities to effectively setup even the most complicated processes in few minutes. The entire setup is purely done on CAD geometry (no more meshing concerns!) and requires only process related input parameters.

The defined process layout will be automatically converted to simulation data based on pre-defined templates, offering the possibility to set company standards. These templates can be easily shared with suppliers, ensuring consistent simulation results for specific parts and/or processes. Simulations are performed with the long-time industrially proven Sheet Metal Forming (PAM-STAMP) solver, to ensure the highest result quality and thus the best predictive confidence.


How to Download

  • Click the Download button
  • Continue to Keysight Software Manager to download Software Updates

Licensing

  • Requires a License

Supporting Documentation

Installs on: PC

Operating System

  • Windows 64

Prerequisites

Downloads

Stamping 2023.5 Solver for Windows

File Size: 860.69 MB
MD5: 51ce672025bd9b707c69cfe15bdd8b71
Info:

BODY MANUFACTURING STAMP 2023.5  for Windows including Visual-Environment 2023.5 and CSM Solver 44.2.0

How to install:

Unzip BMStamp2023r5_Windows.zip in a temporary directory and execute setup.exe

BM-Stamp 2023.5 (Visual-Environment GUI 2023.5) for Windows

File Size: 3.08 GB
MD5: d9bfd472b25e1fd44866228fd329323f
Info:

BM-Stamp 2023.0 (Visual-Environment GUI 2023.5) for Windows 10 64-bit Operating Systems.

How to install:

Unzip VisualEnvGui20235_Windows.zip in a temporary directory and execute setup.exe

SHOW MORE