How to Log Intermittent Voltage Changes During Troubleshooting

Portable Multimeter
+ Portable Multimeter

Identify Intermittent Supply Voltage Changes

Industrial control systems can develop intermittent operating faults when power supplies or connected circuits experience unexpected voltage changes. A programmable logic controller (PLC) input module may behave inconsistently if its supply voltage drops during operation, while other equipment may appear normal when a technician investigates. Because these disturbances can be irregular, a single voltage measurement may show a normal value even when operators have observed repeated faults. Troubleshooting becomes more challenging when several control devices share a supply, equipment cycles through different operating states, or the symptom cannot be reproduced on demand. Technicians must determine whether the reported behavior coincides with a change in supply voltage or originates elsewhere in the system, without assuming that every equipment fault is caused by the power source.

Investigating these conditions calls for observing voltage behavior across a period of equipment operation rather than relying only on isolated readings. Relevant measurement points might include a DC supply output or the voltage delivered to a control circuit, depending on where the fault is suspected. A useful record captures the timing and magnitude of changes so technicians can compare electrical behavior with equipment events, such as a restart, unexpected stop, or alarm. Consistent test conditions matter because normal load changes can also affect measured voltage. Measurement intervals and triggering criteria must suit the disturbance being investigated; events shorter than the recording interval may be missed. Examining the pattern can help technicians identify recurring dips, narrow the likely fault location, and decide where further tests are needed.

Intermittent Voltage Logging Solution

Investigating intermittent voltage changes involves measuring a supply or control-circuit voltage while equipment operates under normal conditions. Instead of relying on a single spot reading, technicians record measurements over time and examine the trend for changes that correspond to reported faults. The recording interval and event settings should be chosen with the duration of the disturbance in mind, since short events may not be captured. Keysight handheld digital multimeters with supported data-logging functions allow technicians to collect voltage readings during field maintenance and review them to investigate intermittent behavior. For extended monitoring in demanding field conditions, available models provide up to 800 hours of battery life, IP67 water and dust resistance, and protection against drops of up to 10 feet. For supported instruments, interval logging builds a time-based measurement history, while event logging can record changes according to the meter's criteria. Technicians can use this record to compare voltage behavior with equipment operating conditions and guide follow-up checks at the power supply, wiring, or control circuit. Logging supports fault investigation but does not replace a faster instrument when brief transients must be captured.

See Block Diagram of Intermittent Voltage Logging Solution

How to Log Intermittent Voltage Changes During Troubleshooting

Explore Products in Our Intermittent Voltage Logging Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?