Supplying DC Bias Source for Optical Device Testing

Demos

Optical devices play a fundamental role in modern data centers by efficiently converting electrical and optical signals. Increasing demands for higher speeds, smaller size, and increased data traffic, are driving the development of highly integrated optical devices. These advanced devices integrate multiple functions and components into a single unit, facilitating efficient system miniaturization. 

 

Testing highly integrated optical devices requires a significant number of precision bias sources. For example, testing integrated tunable wavelength lasers requires precision current sources for the laser diodes to ensure stable optical performance. It also requires precision bias sources for each heater to adjust wavelength precisely. Similarly, coherent optical transceivers require multiple precision bias sources precisely synchronized to the phase control electrodes to convert electrical signals to optical signals accurately.

 

A detailed characterization with very fine bias sweeping steps is necessary to test the optical power and wavelength of tunable lasers and coherent receivers. As a result, issues such as significant extension of test time and unintended wavelength shifts due to thermal effects occur. One effective solution is minimizing each sweep step's duration, enabling faster sweeping and helping mitigate these issues.

 

Challenges in testing optical devices:

 

1. Increasing Channel Density

Highly integrated optical devices have more test ports and components, necessitating a substantial number of high-precision power supplies and significant space. For instance, integrated tunable lasers need precision current sources for the laser diodes to ensure stable optical performance; and precision bias sources for each heater to adjust wavelength precisely. Coherent optical modulators require multiple precision bias sources precisely synchronized to the phase control electrodes to accurately convert electrical signals to optical signals.

 

2. Precision Requirements

The major challenge is the precision required in controlling bias voltage and current. Optical devices, inherently sensitive to variations in biasing, demand a level of precision that pushes the limits of conventional testing equipment. Achieving and maintaining the necessary precision is challenging due to the low tolerances and dynamic nature of optical components.

 

3. Dynamic Operating Conditions

Datacenter environments are dynamic, with fluctuations in temperature, power, and signal conditions being the norm rather than the exception. Maintaining a stable DC bias under these dynamic operating conditions presents a significant challenge. Optical components need to operate reliably and consistently, even when subjected to rapid changes in bias levels – and the need to test these is paramount.

 

4. Non-Linear Behavior of Modulators

Modulators, a critical component in optical communication systems, exhibit non-linear behavior that complicates the testing process. Traditional testing equipment may struggle to accurately capture and replicate the intricate modulation characteristics, leading to potential inaccuracies in assessing the performance of modulators under realistic operating conditions.

 

5. Sensitivity of Receivers

Optical receivers, responsible for converting optical signals into electrical signals, are highly sensitive to variations in bias levels. Achieving a stable and accurate bias for receivers is a delicate task, as even slight deviations can impact signal quality and, consequently, the reliability of the entire communication system. Accurately capturing the significant current variations corresponding to light will also be an extremely challenging task.

 

6. Real-World Simulation

Simulating real-world scenarios in the lab environment is a challenge in itself. Engineers must ensure that the testing conditions accurately reflect the complexities of datacenter operations. This includes simulating the varying conditions optical components may encounter in a live datacenter, from changes in load to fluctuations in ambient temperature.

 

In summary, the challenges in DC bias testing for optical components in datacenters span density, precision, dynamic conditions, non-linear behaviors, sensitivity, high-speed demands, and the need for realistic simulations. Addressing these challenges requires innovative approaches and specialized equipment, making the role of source measure units (SMU) crucial in overcoming these complex hurdles. In this demo video, learn how to use an SMU to provide a precision DC bias source to the device under test while navigating the above-mentioned challenges.