E19-5jtw1
CVSS:
8.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
2
Year:
2018
Description
This strike exploits a buffer overflow vulnerability in tiffcp component of libtiff.
The vulnerability is due to insufficient input validation of an unknown TIFF header field .
A remote attacker could exploit this vulnerability by enticing a user to import a specially crafted TIFF file.
Successful exploitation could lead to arbitrary code execution or denial-of-service conditions in the context of the user.