Samsung DVR Authentication Bypass

Strike ID:
B13-5rl01
CVSS:
5.0 (AV:N/AC:L/Au:N/C:P/I:N/A:N)
False Positive:
f
Variants:
43
Year:
2013

Description

This strike identifies a vulnerability in Samsung DVR Firmware v1.10. An authentication bypass is possible because of improper validation of CGI page requests. If an HTTP request is made to one of many URI paths with a malicious cookie value set, then access will be given to the attacker with the ability to perform many functions such as read usernames and passwords, create users, and read and modify device configuration settings.

CVE