Overview

This E5062.tlb library enables the auto complete function on the external PC. If you use the Microsoft Office applications (Microsoft PowerPoint etc.), as it is equipped with VBA, you can complete the most part of application development within the Microsoft Office applications.

NOTE: The "E5062.tlb" library enables edit only. COM objects for the ENA-L can not be executed.

Operating Conditions

E5061A Rev.A.02.00 only

E5062A Rev.A.02.00 only

Install Procedures

Step1. Download the "E5062.tlb"file.

Step2. Save the "E5062.tlb" to the hard disk drive of your PC (Anywhere is ok).

For more details, refer to the manual on the bottom of this page.