eBooks
Grid modernization is accelerating across the United States, but modernization momentum increasingly depends on deployment confidence. This report, based on third-party market research conducted by Frost & Sullivan and commissioned by Keysight Technologies, examines how distributed energy resources (DER), inverter-based resources (IBR), battery energy storage, smart inverters, electric vehicle charging, advanced communications, and grid cybersecurity requirements are reshaping the way power grid technologies must be tested, validated, integrated, and operated.
The findings show that the grid modernization community is confident in the direction of progress, but less certain that existing validation approaches can scale fast enough to support real-world deployment. As more solar, wind, and battery storage connect through inverter-based power electronics, grid dynamics are changing. Traditional one-way power flow is giving way to bidirectional power flow, system inertia is reduced, and control response windows are compressed. These changes create new requirements for grid simulation, grid emulation, electromagnetic transient modeling, digital twins, grid-edge visibility, low-latency communications, cyber-physical co-simulation, and grid resilience.
For DER and IBR manufacturers, the report identifies a widening gap between product innovation and validation capacity. Manufacturers are developing more capable smart inverters, battery energy storage systems, grid-edge devices, and software-defined energy technologies. Yet each new feature, firmware release, cybersecurity requirement, and interconnection rule expands the test burden. The report highlights that DER and IBR manufacturers face significant resource constraints, cybersecurity and network visibility gaps, and compliance testing challenges. This points to a growing need for automated test workflows, grid simulator capabilities, grid emulator solutions, and repeatable validation environments that help manufacturers prove that products remain compliant, secure, and grid-ready across many operating scenarios.
For system integrators, the report shows that integration confidence depends on more than connecting devices. System integrators play a central role in bringing together DER, IBR, battery storage, communications networks, cybersecurity controls, utility applications, and multi-vendor grid-edge systems. However, their top challenges include cyber testing gaps, resource constraints, and grid simulation issues. These findings highlight the need for stronger grid cybersecurity and network visibility, reusable validation frameworks, and realistic grid emulation before field rollout. As grid infrastructure becomes more software-defined, system integrators must validate evolving software, communications, controls, protocols, and cybersecurity exposure while keeping pace with firmware updates, device additions, field deployment conditions, and changing utility requirements.
For utility and network operators, the report highlights a more cautious view of grid modernization preparedness. Operators are closest to live grid reliability and ultimately carry the operational risk when new technologies enter the field. Their highest-severity testing barriers include grid simulation gaps, interoperability issues, and resource constraints. These challenges underscore the need to validate how DER and IBR systems, grid assets, communications networks, monitoring platforms, and control systems behave under real operating conditions before changes affect the live grid. For operators, grid resilience depends on more than asset deployment. It depends on confidence that connected systems can perform reliably, securely, and predictably under dynamic load changes, grid disturbances, severe weather, communications impairments, cyber events, and multi-vendor interoperability conditions.
The report also explores the growing importance of standards compliance as a foundation for grid modernization. As distributed energy resources, inverter-based resources, battery storage, electric vehicle infrastructure, and grid-edge communications become more deeply embedded in the power system, standards compliance is shifting from a certification checkpoint to a core engineering discipline. Respondents cited challenges across IEEE 1547, UL 1741, IEC 61850, IEEE 2030.5, NERC inverter-based resource reliability requirements, and Critical Infrastructure Protection cybersecurity standards. Recurring pain points include traceability and documentation, evolving requirements, communication protocol compatibility, secure authentication, maintaining test models, mapping systems to regulatory categories, and gathering performance data for inverter-based resource behavior.
A key theme across the report is that grid modernization is not constrained by a single weak link. DER and IBR manufacturers, system integrators, and utility and network operators each face different challenges, but those challenges converge around the same core issue: the grid ecosystem needs a more coordinated way to validate complex, connected, software-driven systems before they reach the field. As solar photovoltaic systems, energy storage, smart inverters, connected appliances, electric vehicle supply equipment, electric vehicles, distributed energy resource management systems, advanced distribution management systems, supervisory control and data acquisition systems, outage management systems, advanced metering infrastructure, and fault location, isolation, and service restoration systems interact more closely, grid operation increasingly depends on the interaction between power flows and data communications.
This report argues that the next phase of grid modernization requires a shift from fragmented testing to shared validation confidence. Grid simulator and grid emulator technologies, combined with software simulation, power hardware-in-the-loop testing, communications emulation, protocol validation, cybersecurity assessment, and network visibility, can help the industry test systems earlier and more realistically. Grid simulation and grid emulation are especially important because many of the most consequential failure modes do not appear when devices operate in isolation. They emerge when power, communications, software, cybersecurity, and control systems interact under real-world conditions.
For organizations involved in grid modernization, the message is clear: progress is real, but deployment confidence must be earned through more rigorous validation. Manufacturers need to scale product validation despite resource limits, cybersecurity visibility gaps, and compliance demands. System integrators need repeatable ways to validate multi-vendor systems under realistic grid and communications conditions. Utility and network operators need stronger confidence that modernization can be trusted in live operations. Together, these needs point to a more integrated validation model built around grid simulation, grid emulation, grid cybersecurity, interoperability testing, standards traceability, and operational visibility.
By examining the validation challenges facing DER and IBR manufacturers, system integrators, and utility and network operators, this report provides a practical view of what the grid modernization ecosystem must solve next. The future grid will be more distributed, software-defined, communications-dependent, and cyber-exposed. Its success will depend not only on new infrastructure investment, but on the ability to validate that modern grid technologies can operate together safely, securely, and reliably at scale.
What are you looking for?