Personalized Support Helps 5G Device Test Master New Tests in Hours

Case Studies

Consumer demand for wireless network capacity, availability, and speed drives the 5G ecosystem. Nowhere is the pressure more intense than in 5G device development, where first-to-market advantage provides substantial opportunities for share gain or loss in each cycle. Teams developing 5G devices must master a wide range of constantly evolving standards and tests for those standards. Standards evolution reaches far beyond radio interface, touching every system in the phone, including RF conformance and interface standards for I/O, memory, and compute

 

Though USB compliance testing has existed since 1995, an older standard does not mean a simple one. In particular, policies and procedures related to the USBIF Certification Program continue to change

 

New devices must meet these test standards, which come with new techniques that require new equipment and processes. The application development team must understand these standards to ensure that its 5G solutions achieve design specifications and logo certifications

 

Company:

• 5G device developer

 

Key issues:

• master unfamiliar USB 2.0 compliance test

• rapidly learn new test instrument

 

Solutions:

• remote demo with overview of test setup and procedures

• real-time access to USB compliance test experts

 

Results:

• reduced learningrelated delays by > 2 days

• avoided $200,000 in lost productivity

 

Challenge: An Updated Standard. A New Instrument. A New Test Matrix

 

To test the USB interface, the wireless application development team at a 5G device development company needed to add a piece of equipment to its bench. It purchased a Keysight 81160A pulse function arbitrary noise generator for USB 2.0 receiver compliance testing. The pulse-pattern generator has all the necessary tools to measure real-life data sequences for high-speed serial buses and generate the data packets for digital bus device tests. One test verifies the sensitivity of a device’s receivers on both the upstream and downstream data ports in noisy environments. It’s important to perform the test correctly

 

The team knew the deadline for completing the USB 2.0 receiver sensitivity test loomed, threatening to compromise its tight schedule. Though this was a well-understood technology, the team did not know how to perform these new test procedures. With schedules tight and pressure high to test the device to multiple standards, the application developers could not afford to spend engineering time on trial-and-error testing. With a new piece of equipment and an unfamiliar standard test procedure, it would take days to figure it out on their own

 

Solution: Personalized Support with Fast Access to a Team of Experts

 

Faced with the challenges of a new instrument and a new-to-them compliance standard, the 5G application developers turned to a trusted partner, Keysight

 

Unknown to the team, when the company purchased the 81160A pulse function arbitrary noise generator, it received KeysightCare Assured service and support. KeysightCare Assured is a premiere support solution that offers committed four-business-hour technical response, plus repair coverage with 10- business-day repair turnaround time and proactive firmware notifications

 

Getting precise, personalized support accelerated the application developers’ work and propelled them into action in a matter of hours. After articulating their needs, they connected with a KeysightCare application engineer, who scheduled a live remote demonstration to provide support tailored to their specific requirements

 

Over WebEx, the KeysightCare application engineer remotely demonstrated how to configure the 81160A for the required USB 2.0 receiver testing. The customer watched the demonstration remotely, learning how to successfully test both standard and nonstandard USB 2.0. The KeysightCare hardware and software engineers supporting the customer received training in the latest USB specifications and test requirements, including the USB 2.0 compliance test update from February 2020. Expertise on the latest standards proved critical in resolving the customer’s need quickly

 

In addition, the KeysightCare application engineer recorded notes in the KeysightCare portal for future reference by the customer’s 5G application development team

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.