Samtec Reduces R&D Lab Test Time from Four Hours to Five Minutes

Case Studies

Samtec, a leading provider of high-speed interconnect solutions, has successfully reduced its R&D lab test time from four hours to five minutes by using Keysight’s 32-port 53 GHz vector network analyzer (VNA) with N1930B Physical Layer Test System (PLTS). This solution enables Samtec to optimize serial channel integrity for a controlled impedance environment and achieve 50% faster time to market for its next-gen 112 Gbps PAM4 interconnect solutions. Keysight’s 32-port M9808A PXIe VNA with N1930B PLTS is the only instrument on the market that provides frequency domain, time domain, eye diagrams, multichannel simulation, and W-element modeling in a single test bed platform. It uses highly accurate calibration techniques coupled with an intuitive graphical user interface to expedite the test flow. It also produces ultra-stable measurements with high dynamic range, providing accurate test data at very low crosstalk signal levels. To learn more about how Keysight’s VNA system can help high-speed interconnect companies meet the demand of today’s hyperscale data centers, visit www.keysight.com/find/m9808a and www.keysight.com/find/plts. You can also contact your local Keysight office for more information on Keysight’s products, applications or services. The complete list of Keysight offices is available at www.keysight.com/find/contactus.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.