NSS03 RTP measurement system

Solution Briefs

This measurement kit was intended for the evaluation of electric wave absorption materials used for the prevention of oscillation and as an anti-EMI measure in cellular communication devices. In a small container such as a cell phone, the electromagnetic wave tends to be easily distorted, or the electric field and the magnetic field exist independently and disorderly. It is essential for an ideal electric wave absorption material to carry a large electric wave absorption rate in the near field and not to disturb the impedance of the circuit even in such a harsh environment.