The B.01.04 Cable Fault Location Measurement Personality can be obtained using one of the following two methods:

  • If you already have a license for this personality you can download the latest version from this site for free to a Microsoft Windows based Personal Computer.
  • If you do not have a license for this personality you will need to order an E440xBU-225 upgrade kit.

Note: This Cable Fault Location Measurement Personality version is only for use with ESA-E Series Spectrum Analyzers with firmware version A.07.01 or newer.

The "ESA Personality Installation Procedure" will guide you through:

  • Downloading the installation image
  • Creating an installation floppy disk set
  • Loading the software into your ESA
  • Verifying the installation
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2008-02-12 B.01.04 Downloadable installation file...
Release Date Version
2008-02-12 B.01.04
Version Description
Downloadable installation file...

How to Download

  • See the Installation Procedure

Licensing

  • Requires a License

Installs on: PC / Instrument

Prerequisites

  • See the Installation Procedure

Supported Instruments

  • E440xBU 225
No previous versions available
SHOW MORE