Joomla Component Proclaim Backup File Download

Strike ID:
E18-0omt1
CVSS:
7.5 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:N/A:N
False Positive:
f
Variants:
2
Year:
2018

Description

This strike exploits a file download vulnerability in Joomla! Component Proclaim The vulnerability is due to the improper sanitization of requests sent to the application. An attacker could download sql files under backup folder via direct requests.

CVE