WordPress Marketplace Remote Code Execution

Strike ID:
E14-zv2t1
CVSS:
8.8 CVSS:3.1/AV:N/AC:L/PR:L/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2014

Description

This strike exploits a RCE vulnerability existent in the WordPress Marketplace plugin. This vulnerability is due to the lack of proper input sanitization while processing data from a POST request. An unauthenticated user could exploit this vulnerability by specially crafting a HTTP POST request with a call to wpmp_pp_ajax_call() method, which can lead to arbitrary code execution in the context of the vulnerable WP plugin.

CVE

Bid