E19-0s3x1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2019
Description
This strike exploits a path traversal vulnerability found in Cisco Prime Infrastructure (PI) and Cisco Evolved Programmable Network (EPN) Manager.
The vulnerability is due to improper validation of user-supplied input.
An attacker could exploit this vulnerability by uploading a malicious file to the administrative web interface.
A successful exploit could allow the attacker to execute code with root-level privileges on the underlying operating system.