D21-3dsu1
CVSS:
7.8 CVSS:3.0/AV:L/AC:L/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
2
Year:
2017
Description
This strike exploits a code execution vulnerability in Microsoft Outlook 2010.
The vulnerability is due to improper handling of objects in memory or Microsoft Outlook security feature bypass vulnerability.
By setting a crafted HTML page as Home Page in Outlook 2010, allows the attacker to execute code in the context of current user.
Note: This strike simulates the opening of a malicious page at address defined in Outlook (Home Page).