Using BenchVue Software’s Test Flow Application to Characterize Transistors

Application Notes

This application note shows how to make a simple transistor curve tracer using a Keysight B2962A power source along with a Test Flow sequence running in Keysight’s BenchVue software. The B2962A was chosen because of its low current stimulus capabilities, but BenchVue works with hundreds of Keysight instruments. Many other choices are possible depending upon your measurement requirements.

BenchVue Test Flow

BenchVue Test Flow is a flow-chart style sequencer that is included with purchase of any BenchVue app. It allows you to create automated tests without programming, simply by dragging and dropping properties and measurements into a sequence. It’s not like graphical programming, such as Keysight VEE, because you are not interacting with drivers and having to understand all the nuances of the instruments.