Oracle WebLogic Server Activator Insecure Deserialization

Strike ID:
E18-0l7x1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
2
Year:
2018

Description

An insecure deserialization vulnerability was found in Oracle WebLogic Server. The vulnerability is due to insufficient validation of serialized data within T3 requests. The vulnerability can be exploited by sending a specially crafted serialized object. Successful exploitation can result in arbitrary code execution in the context of the user running WebLogic.

CVE

References

Bid