LibreOffice code execution

Strike ID:
E19-0yaw1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2019

Description

This strike exploits a code execution vulnerability in LibreOffice. The vulnerability is due to unrestricted use of document event function to trigger LibreLogo to execute python contained within a document. An attacker could entice the victim to open the crafted odt file. Successful exploitation could lead to code execution on the victim's machine.

CVE

Bid