Indusoft ThinClient ActiveX Control Initialize2 Method Buffer Overflow

Strike ID:
E13-3vh01
CVSS:
6.8 (AV:N/AC:M/Au:N/C:P/I:P/A:P)
False Positive:
t
Variants:
1
Year:
2013

Description

This strike identifies a vulnerability in an Indusoft ThinClient ActiveX control. The Initialize2 method does not properly validate its arguments. If a malicious or overly large string size is used and exceeds the limit of the buffer, an overflow will occur allowing for remote code to be executed.